Options dialog box: Scheduled Operations

How do I open the Options: Scheduled Operations dialog box?
  1. Select
    Tools > Options
    .
  2. Under
    Category
    on the left side of the dialog box, select
    Scheduled Operations
    .
Use the
Options: Scheduled Operation
dialog box to set the default behaviors for a scheduled asset's operations and scheduled search operations. These settings will be applied to new schedules. Changes to these settings will not affect existing schedules.
The
Scheduled Operations
portion of the dialog box is made up of two sections. On the left is a tree showing the available assets and on the right, the default operations of the selected asset or search.
  • Navigate the Scheduled Operations tree to select the item for which you want to set defaults. For example, navigate to
    Disaster Recovery, Backup, MicroLogix
    to set default operations for Allen-Bradley MicroLogix controllers in backup schedules or navigate to
    Scheduled Search, Search
    to set default operations for scheduled searches.
  • Use the
    Scheduled Operation
    tab and
    Standard
    tab on the right to change the default operations. New settings are enforced when an existing operation is active or run manually.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal