Options dialog box: File Associations
How do I open the Options: File Associations dialog box?
- SelectTools > Options.
- UnderCategoryon the left side of the dialog box, selectFile Associations.
Use the
Options: File Associations
dialog box to have a designated software product open files with a specific extension. If there are no personal or system file associations configured to open files with a specific extension, FactoryTalk AssetCentre will attempt to open files using Microsoft Windows' default file associations.To perform any of the actions below you must have
Configure Personal Archive File Associations
or Configure System Archive File Associations
permission.- Add a file associationOn thePersonal AssociationsorSystem Associationstab, clickNew, complete theFile Associationdialog box, and clickOK.
- Edit a file associationOn thePersonal AssociationsorSystem Associationstab, select a file type, clickEdit, complete theFile Associationdialog box, and clickOK.
- Remove a file associationOn thePersonal AssociationsorSystem Associationstab, select the association and then clickDelete. When the "Are you sure you want to delete the file association for extension .XXX" message appears, clickYes.
Provide Feedback