Edit a file association
To edit a file association,
you must have
.Configure Personal Archive File Associations
or Configure System Archive File Associations
permissionTo edit a file association
- SelectTools > Options.
- UnderCategoryon the left side of the dialog box, selectFile Associations.
- On thePersonal AssociationsorSystem Associationstab, select a file type, and then clickEdit.TheFile Associationdialog box opens.
- TheFile extensionfield is unavailable when you edit an existing file association.
- In theProgramfield, clickBrowseto select the software product to open files with the indicated extension.
- In theCommand Argfield, specify the command line arguments for the software product used to open files of this type.
- In theDescriptionfield, enter the name of the software.TIP:The file name in theProgramfield can be very different than the actual product name. It's recommended to enter the name of the software for clarity.
- Select theAutomatically check in file or asset after editingbox if you want files of this type to be automatically checked in when the editing program is closed.
- After you select theAutomatically check in file or asset after editingbox, theMonitor Typefield becomes available.
- ChooseFilefor RSLogix 5, RSLogix 500, RSLogix 5000, Logix Designer, Microsoft Word, and Microsoft Excel.
- ChooseProcessfor Microsoft Notepad, Microsoft WordPad, FactoryTalk View ME (.mer), DriveTools (.dno), PanelBuilder (.pva), and the Siemens S7 Controllers (STEP7) editor.
- ClickOK.
Provide Feedback