File Association dialog box
How do I open the File Association dialog box?
- SelectTools > Options.
- In theOptionsdialog box underCategoryon the left, selectFile Associations.
- Click thePersonal Associationstab or theSystem Associationstab, and then:
- ClickNew.
- Or, select a file extension in the list and clickEdit.
Use the
File Association
dialog box to manage file associations that determine which software product opens a particular file type.With the
File Association
dialog box, you can specify the following configurations:- File extension to be opened by the designated software product
- The software product to open files with the indicated extension
- Command line arguments for the software product used to open files
- The name of the software
- If files of this type is automatically checked in when the editing program is closed.
- Monitor type
Provide Feedback