Set file associations

You can determine the software product that opens a particular type of file. For example, if you associate files that have a .txt extension with your favorite text editor (for example, Microsoft Wordpad), Wordpad will open all files with the extension .txt. If you do not set file associations, the default Windows associations will be used.
For a binder, set the file association for the key file in the binder.
Prerequisites
  • To set system file associations, you must have
    Configure System Archive File Associations
    permission.
  • To set personal file associations, you must have
    Configure Personal Archive File Associations
    permission.
To set file associations
  1. Select
    Tools > Options
    .
  2. In the
    Options
    dialog box under
    Category
    , select
    File Associations
    .
  3. In the
    Options
    dialog box: File Associations, click the
    Personal Associations
    or
    System Associations
    tab, and click
    New.
    The
    File Association
    dialog box opens.
  4. In the
    File extension
    field, specify the file extensions (for example, acd, ccwsln, and rss) to be opened by the designated software product.
  5. In the
    Program
    field, click
    Browse
    to select the software product to open files with the indicated extension.
  6. In the
    Command Arg
    field, specify the command line arguments for the software product used to open files of this type.
  7. In the
    Description
    field, enter the name of the software.
    TIP:
    The file name in the
    Program
    field can be very different than the actual product name. It's recommended to enter the name of the software for clarity.
  8. Select the
    Automatically check in file or asset after editing
    box if you want files of this type to be automatically checked in when the editing program is closed.
  9. After you select the
    Automatically check in file or asset after editing
    box, the
    Monitor Type
    field becomes available.
    • Choose
      File
      for RSLogix 5, RSLogix 500, RSLogix 5000, Logix Designer, Microsoft Word, and Microsoft Excel.
    • Choose
      Process
      for Microsoft Notepad, Microsoft WordPad, FactoryTalk View ME (.mer), DriveTools (.dno), PanelBuilder (.pva), and the Siemens S7 Controllers (STEP7) editor.
  10. Click
    OK
    .
    TIP:
    When setting file associations you can also turn on the automatic check-in feature for that file type. When this feature is turned on, files will be checked in automatically after the file is edited.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal