Column headings on the Personal and System Associations tabs
The column headings on the Personal and System Associations tabs are the same. They include:
- ExtensionThe three-letter part of a file name that follows the period and designates the type of file. For example, the fileboiler.rspis an RSLogix 5 project file.
- ProgramThe software product that should be used to open the file type in theExtensioncolumn. The executable program file is shown here. For example,RS500.exe.
- Command ArgsCommand line arguments for the software product that will be used to open files of this type. Command line arguments are used to specify a particular behavior when a program is run from the Windows Command Prompt. For example, if you start Microsoft Word 2007 from the Command Prompt, you can use the/qcommand line argument to start Word without showing the splash screen:C:\Program Files\Microsoft Office\Office12\Winword.exe /qIn the context of FactoryTalk AssetCentre, command line arguments are used when a file in Archiveis opened using the associated software. For example, you can use the/presetcommand line argument to open the project file in the RSTune Faceplate software for trend analysis.Refer to the software program's documentation to find out what command line arguments are available in that software.
- DescriptionA description of the file association. The file name shown in theProgramcolumn can be very different than the actual product name. Usually theDescriptioncolumn contains the name of the software for clarity. For example, a description ofRSLogix 500explains the filename of RS500.exe.
- Auto Check-InIndicates whether the automatic check-in feature is enabled or disabled for this file type. When automatic check-in is enabled, a file of this type will be automatically checked in when editing is finished. Depending on the Monitor Type, the file will be checked in when the file is closed or when the associated program that was used to edit the file is closed.
- Monitor TypeThis column is only relevant if theAuto Check-Incolumn showsEnabled. It has to do with how FactoryTalk AssetCentre determines when to automatically check in a file.
Provide Feedback