Remove a file association
To remove a file association, you must have
Configure Personal Archive File Associations
or Configure System Archive File Associations
permission.To remove a file association
- SelectTools > Options.
- UnderCategoryon the left side of the dialog box, selectFile Associations.
- On thePersonal AssociationsorSystem Associationstab, select the association, and then clickDelete.
- When the messageAre you sure you want to delete the file association for extension .XXXappears, clickYes.
Provide Feedback