Options dialog box: Database Limitations

How do I open the Options: Database Limitations dialog box?
  1. Select
    Tools > Options
    .
  2. Under
    Category
    on the left side of the dialog box, select
    Database Limitations
    .
Use the
Options: Database Limitations
dialog box to specify the settings of database limitations, including:
  • Total maximum size of the AssetCentre database
  • Size warning levels
  • Maximum number of versions per archive asset
  • Maximum size of database table capturing logs
  • Database capacity status refresh rate
  • Email notification
By default, the
Database Limitations Enabled
check box is not selected, and all the settings of database limitations are unavailable. To select the
Database Limitations Enabled
check box to configure all the settings, you must have
Configure Database Limitations
permission.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal