Options dialog box: Change Detect
How do I open the Options dialog box: Change Detect dialog box?
- SelectTools>Options.
- UnderCategoryon the left side of the dialog box, selectChange Detect.
Use the
Options: Change Detect
dialog box to configure the communication settings
between FactoryTalk AssetCentre agent and controllers when performing a change detect
task, including the number of concurrent monitoring tasks and the packet size used to
read the controller logs when changes are detected:
TIP:
These overall settings can only be modified via
FactoryTalk AssetCentre Desktop
Client
> Tools
> Options
or FactoryTalk AssetCentre Web
Client
> Tools
> Change Detect
. Any changes made will apply
only to new schedules and do not affect existing ones. To apply updated overall
settings to previous change detect schedules, deactivate the old schedules first,
and then activate them again.- Concurrent of monitoring tasksEnter the number of concurrent monitoring tasks used for communication between FactoryTalk AssetCentre and the controller. The value must be between 2 and 64, with a default of 32. To use system resources efficiently, consider the number of controllers involved in your change detect schedules when setting this value:
- For a high number of controllers, for example, 100, setting this to the maximum of 64 enables faster scanning across more controllers at once, but the remaining 36 tasks will be queued.
- For a low number of controllers, for example, 2, setting this to 2 ensures that no excess tasks are opened unnecessarily, helping conserve system resources.
- Connection typeConfigure the packet size used to read the controller logs when changes are detected. For example, if the size of a change log entry is 2000 bytes, whenUse 4000-byte packet connection (reduce network traffic)is selected, a change log entry can be retrieved in one read. IfUse 500-byte packet connection (for compatibility)is selected, retrieving a change log entry requires four reads. By default, theUse 500-byte packet connection (for compatibility)option is selected.WARNING:Using 4000-byte packet connection option is faster and more efficient, but it can also consume more system resources and impact motion on a controller.
- Use 500-byte packet connection (for compatibility)
- Use 4000-byte packet connection (reduce network traffic). To use this option, the following minimum versions are required:
- Controller firmware revision 20 or later when using the controller’s built-in Ethernet port.
- Ethernet communication module firmware revision 5 or later when using an Ethernet communication module.
- FactoryTalk Linx software version 6.60 or later.
Provide Feedback