Working with Trusted Applications
Trusted
ApplicationsThe
AADvance-Trusted SIS Workstation software®
is the development environment that enables the creation of one comprehensive project to control a Trusted®
controller. The AADvance-Trusted SIS Workstation software
enables the creation of Trusted
applications supporting multi-process control. Applications consist of virtual machines running on hardware components. The development process consists of creating a project made up of one device, representing the hardware, which is then downloaded to the Trusted
controller. At runtime, the device becomes a virtual machine running on the hardware equipment.Develop projects with these programming languages from the IEC 61131-3 standard: Functional Block Diagram (FBD), Ladder Diagram (LD), and Structured Text (ST). When building, the compiler produces "target independent code" (TIC).
Develop projects on a
Windows®
development platform. The AADvance-Trusted SIS Workstation software
graphically represents and organizes the device and program organization units (POUs) within a project from many views.Choose to simulate the running of a project, after building a project, with high-level debugging tools, before actually downloading the device to the
Trusted
controller. Then connect the AADvance-Trusted SIS Workstation software
to monitor real-time information and perform updates. Use a standard Ethernet or serial network to connect the AADvance-Trusted SIS Workstation software
with the Trusted
controller.Provide Feedback