ISaVIEW
Create graphical interfaces or
ISaVIEW
screens to monitor or run control processes
on local computers or remote locations that use Internet or network connections. Add
ISaVIEW
screens to projects at the device and program level.Create and develop
ISaVIEW
screens while editing a project or running online
(simulation or debugging). To develop ISaVIEW
screens, insert graphic objects and
define animation behaviors for execution at run-time.Create
ISaVIEW
screens from blank documents or from a template. Insert objects
available from the Toolbox
. Modify object properties to define animation effects.
Also group objects together, then define animation effects for the group.While running online, switch between design mode and animation mode. Design mode to edit
objects contained in screens. Animation mode launches the execution of animation effects
defined for objects contained in screens.
From the
ISaVIEW
toolbar, perform these operations:Operation | Description |
|---|---|
![]() | Design Mode, edit objects contained in screens while connected (simulation or
online) |
![]() | Animation Mode, launch the execution of animation effects defined for objects
contained in screens while connected (simulation or online) |
![]() | No Preview, graphically edit objects contained in a screen without displaying
any animation effects. Modify, add, delete, move, group, or ungroup objects. |
![]() | Preview Selection, visualize some animation effects defined for selected
objects in a screen |
![]() | Preview Animation Effects (Editable), visualize and graphically modify some
animation effects defined for all objects contained in a screen. Does not enable to
modify, add, delete, move, group, or ungroup objects. |
![]() | Group Selection, group selected objects |
![]() | Ungroup Selection, dissociate a selected group of objects |
Provide Feedback