Export an ISaVIEW screen as a template
Develop an
ISaVIEW
screen then export the screen for use as a template with the *.hmi extension. The default names of templates are the same as the screen names. When adding an ISaVIEW
screen from a template, choose from the available templates. ISaVIEW
templates are stored here:%USERPROFILE%\AppData\Local\Rockwell Automation\SIS Workstation
<version>
\ACP\Templates\IsaviewTo export an ISaVIEW screen as template
- Develop anISaVIEWscreen.
- From theApplication View, right-click theISaVIEWitem, and then clickExport as Template.
- In theExport ISaVIEW Templatedialog box, type the template name, and then clickOK.
Provide Feedback