Define Animation Effects for Objects
Define animation of these effects for objects or groups of objects defined in
ISaVIEW
screens:- Action
- Color
- Displacement
- Rotation
- Size
- Text
- Visibility
Set property values from the
Properties
window to define animation effects. Also switch to the animation preview mode to graphically modify the rotation, displacement, and size properties.All global and local variables are available to set the properties in the
Properties
window. The Collection
Editor
is available to define the color property Fill
Color
Phase
and the text property Text
Color
Phase
. Use the Collection
Editor
to create and edit the members of a collection and to define the colors (Phase
Colors
) and numerical values (Phase
Maximum
and Phase
Minimum
) for each member. When online, the object or object text displays the color that corresponds to its current value as defined in the collection. Example: for the color black, assign a value of 10 to Phase
Maximum
and a value of 0 to Phase
Minimum
displays the object or object text as black when its value is between 0 and 10.Provide Feedback