Displacement
Define displacement properties for all
ISaVIEW
objects. Before displacement occurs, the coordinates of the upper left corner of the object define the start position. Use the displacement properties to define the linear movement of the object when in animation mode. Define displacement properties from the Properties
window. Also, define the Animation Position
property within the workspace. These properties define the displacement of an object:Property | Description |
|---|---|
Animation Position | Destination coordinates after displacement during animation mode in reference to the top left corner of the object bounding box, in pixels (design mode displays InitialPosition coordinates). |
Displacement Variable | Variable that controls the object displacement. Possible variable data types are DINT or STACKINT. Click to select a variable. |
Initial Position | (Read only) Coordinates of the object prior to displacement. |
Location | Actual coordinates of the object. Equal to Initial Position while in design mode. |
Maximum Displacement | Maximum amount of displacement during animation mode. The default value is 1000. |
Minimum Displacement | Minimum amount of displacement during animation mode. The default value is 0. |
In animation mode, the final position of the object is defined as:
Initial Position + (Animation Position - Initial Position) * [(Displacement Variable - Minimum Displacement) / (Maximum Displacement - Minimum Displacement)]
Define displacement properties for an object from the Properties window while in design mode.
To define the displacement properties of an object
- Click
to set the ISaVIEWscreen to design mode. - Select the required object or group of objects.
- In thePropertieswindow, define the required displacement properties.
Provide Feedback
to select a variable.