Visibility
Define the visibility property for individual
ISaVIEW
objects.
Define the visibility property in the Properties
window. This property defines the
visibility of an object:Visibility Variable | Variable that controls the visibility of the object. Possible variable data
type is BOOL. Click to
select a variable. |
To define the visibility property of an object
- Click
to set the
ISaVIEWscreen to design mode. - Select the required object or group of objects.
- From thePropertieswindow, define the visibility property.
Provide Feedback
to
select a variable.