Insert Objects

Insert these objects into an
ISaVIEW
screen from the
Toolbox
.
  • Arc
  • Arrow
  • Ellipse
  • Rectangle
  • Rounded Rectangle
  • Triangle
  • Image
  • Web Container
  • Button
  • Edit Box
  • Gauge
  • Slider
  • Line
  • Bar Meter
  • Polygon
Overlap or superimpose objects and groups of objects. Use contextual menu options to group objects and move objects to the front or back.
TIP: Web containers always remain on top of other objects.
By default, only the basic properties display in the
Properties
window for
ISaVIEW
objects.
To display the extended properties for an ISaVIEW object
  1. From the
    View
    menu, click
    Properties
    Window
    .
  2. In the
    Properties
    window, click isv_exp.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal