Edit Box
The edit box object enables to display and enter text and has a rectangular shape. Define the properties for the edit box object from the
Properties
window. For the edit box object, define properties for Action
, Color
, Displacement
, Size
, Text
, and Visibility
. Also choose to display a border to outline the edit box:Property | Description |
|---|---|
Border | The object has a border. Possible values are True or False. |
To insert an edit box
- From theToolbox, drag the edit box object into the workspace.
Provide Feedback