Image
The image object holds file formats such as GIF, JPEG, BMP, PNG, and TIFF. Image objects cannot be rotated.
Define the properties for the image object from the
Properties
window. For the image object, define properties for Action
, Displacement
, Size
, Text
, and Visibility
. The image object also has the Image
Path
property.Property | Description |
|---|---|
Image Path | Path to the image to display |
To insert an image
- From theToolbox, drag the image object into the workspace.
Provide Feedback