Rectangle
A rectangle represents, for example, pipes that indicate a flow from one object to another with a change of color or a container that displays a changing quantity of liquid as it flows to or from another object. Define properties for the rectangle object from the
Properties
window. For the rectangle object, define properties for Action
, Color
, Displacement
, Rotation
, Size
, Text
, and Visibility
. The rectangle also has frame color and width properties.Property | Description |
|---|---|
Frame Color | Color for the frame of the object. Possible colors are custom, web, and system colors. |
Frame Width | Width of the frame for the object. Possible values are literal values. |
Define fill color for objects in the
Color
properties.To insert a rectangle
- From theToolbox, drag the rectangle object into the workspace.
Provide Feedback