Polygon
A polygon object consists of three or more connected straight lines to form a closed figure. Each line is a segment. Define the properties for the polygon object from the
Properties
window. For the polygon object, define properties for Action
, Color
, Displacement
, Size
, Text
, and Visibility
. The polygon also has frame color and width properties.Property | Description |
|---|---|
Frame Color | Color for the frame of the object. Possible colors are custom, web, and system colors. |
Frame Width | Width of the frame for the object. Possible values are literal values. |
Define fill color for objects in the
Color
properties.For polygon objects, establish the end of each segment that forms the shape, then establish the end of the shape upon completion of all segments. Establish the end of a segment.
Use keyboard commands with polygon objects: press
Ctrl+Z
to undo up to the first segment and press Escape to delete a polygon object in progress.To insert a polygon
- From theToolbox, drag the polygon object into the workspace.
- Click and drag to define each segment that forms the shape, then pressEnterto complete the shape.
- To cancel the shape, pressEscape.
Provide Feedback