Line
The line object is a unbroken linear shape. Define the properties for the line object from the
Properties
window. For the line object, define properties for Action
, Displacement
, Rotation
, Size
, and Visibility
. The line also has color and width properties.Property | Description |
|---|---|
Line Color | Color for the line object. Possible colors are custom, web, and system colors. |
Line Width | Width of the line object. Possible values are literal values. |
To insert a line
- From theToolbox, drag the line object into the workspace.
Provide Feedback