Web Container
The web container object has a rectangular shape. Define properties for the web container object from the
Properties
window. For the web container object, define properties for Action
, Displacement
, Size
, Text
, and Visibility
. The web container object also has frame and object-specific properties:Property | Description |
|---|---|
Link Page | Target URI to display in the object |
Frame Color | Color for the frame of the object. Possible colors are custom, web, and system colors. |
The web container always remains on top of other objects in a screen.
To insert a web container
- From theToolbox, drag the web container object into the workspace.
Provide Feedback