Triangle
A triangle object is a triangular shape. Define properties for the triangle object from the
Properties
window. For the triangle object, define properties for Action
, Color
, Displacement
, Rotation
, Size
, Text
, and Visibility
. The triangle also has frame color and width properties.Property | Description |
|---|---|
Frame Color | Color for the frame of the object. Possible colors are custom, web, and system colors. |
Frame Width | Width of the frame for the object. Possible values are literal values. |
Define fill color for objects in the
Color
properties.To insert a triangle
- From theToolbox, drag the triangle object into the workspace.
Provide Feedback