Arc
An arc is any unbroken part of the circumference of a circle. An arc represents, for example, a container that displays a changing quantity of liquid as it flows to or from another object. An arc object consists of a starting angle and an angle length:

Define the properties for the arc object from the
Properties
window. For the arc object, define properties for Action
, Color
, Displacement
, Size
, Text
, and Visibility
. The arc object specific properties are:Property | Description |
|---|---|
Angle Length | Length of the arc in degrees |
Angle Start | Size of the angle prior to the start of the arc |
To insert an arc
- From theToolbox, drag the arc object into the workspace.
Provide Feedback