Rounded Rectangle
A rounded rectangle is a rectangular shape with rounded corners. Define the properties for the rounded rectangle object from the
Properties
window. For the rounded rectangle object, define properties for Action
, Color
, Displacement
, Size
, Text
, and Visibility
. The rounded rectangle also has frame color and width properties.Property | Description |
|---|---|
Frame Color | Color for the frame of the object. Possible colors are custom, web, and system colors. |
Frame Width | Width of the frame for the object. Possible values are literal values. |
Corner Radius | Radius of the corners for a rounded rectangle. Possible values are literal values. |
Define fill color for objects in the
Color
properties.To insert a rounded rectangle
- From theToolbox, drag the rounded rectangle object into the workspace.
Provide Feedback