Create an ISaVIEW screen from a blank document
Create an
ISaVIEW
screen from a blank document, then insert objects from the Toolbox
and define animation effects. Export screens as templates for reuse.To create an ISaVIEW screen from a blank document
- From theApplication View, right-click the controller or program, point toAdd, and then clickNew ISaVIEW.
- Double-click the addedISaVIEWscreen.TheISaVIEWscreen appears.
- Insert objects and define animation effects.
Provide Feedback