Create an ISaVIEW screen from a template

Create an
ISaVIEW
screen from an existing
ISaVIEW
template.
ISaVIEW
templates have the *.hmi extension.
To create an ISaVIEW screen from a template
  1. From the
    Application View
    , right-click the controller or program, point to
    Add
    , and then click
    ISaVIEW from Template
    .
  2. In the
    Select the ISaVIEW Template
    dialog box, browse to locate the required template, and then click
    Open
    .
  3. In the
    Import ISaVIEW Template
    dialog box, specify a screen name and associate the required variables where required, and then click
    OK
    .
  4. Double-click the imported
    ISaVIEW
    screen.
    The
    ISaVIEW
    screen appears.
  5. Edit and insert objects, and then define animation effects.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal