Diary
Each program organization unit (POU) in a
Trusted®
application includes a Diary file. The Diary text file enables adding notes and comments for each POU in a project. Add or modify information at any time. When copying and pasting a POU, the content of the diary file is not copied. Using the
Document Generator
, print the information displayed in the Diary file for selected POUs.To add or modify an entry to the Diary file of a POU
- In theApplication View, expand the node for the required POU, and then double-click<POU>-Diary.
- In theDiarywindow, enter or modify the required information, and then save the Diary file.
Provide Feedback