Activity Logger
To display the Activity Logger
From the Application View, right-click the project, and then click
Activity Logger
.The
Activity Logger
displays major actions and modifications performed in a project. Each entry in the Activity Logger
includes the local date and time of the action or modification and the user name. Importing a Trusted®
Toolset project displays the existing history of modifications in the Activity Logger
, including the original date and time. Imported entries display N/A
instead of the user name.The
Activity Logger
displays a maximum of 10,000 entries. Exceeding the maximum number of entries deletes the oldest entry. Provide Feedback