Legacy Log Entries
When importing a
Trusted®
Toolset project, the Activity Logger lists these types of actions and modifications. All entries include the date, time, and user account that performed the action or modification.Log Entry | Description |
|---|---|
BACKUP | Generate a project archive (*.pia). |
Make application code | Code result when compiling the application code:
|
APPLICATION VERSION NUMBER = # | Version number of the application |
Verify program ' ProgN ' | Code result when verifying the Program Organization Unit (POU):
|
Download application | Download the application to the Trusted controller. |
WARNING: Cannot determine if on-line update is possible | Unable to determine if an on-line update is possible. |
Target requires APPLICATION VERSION NUMBER = # for update | Application version number required to perform an update. |
| Method to use for on-line update:
|
Update application code | Perform an on-line update of the application code running on the Trusted controller. |
Application run time options | Modify the application run time options. |
Setup compiler options | Modify the compiler options. |
IEC1131 TOOLSET - <Project> - Resource definition | Modify the application (resource) definition. |
IEC1131 TOOLSET - <Project> - Project descriptor | Modify the project description. |
IEC1131 TOOLSET - <Project> - I/O connection | Save an I/O connection. |
Conversion tables | Save a conversion table. |
Create project - Name is ' PrjName ' | Create a project. |
Copy project ' PrjName ' to 'NewPrj ' | Copy a project to the new project name. |
Rename project ' PrjName ' as 'NewName ' | Rename the project. |
IEC1131 TOOLSET- < Project:Spotlight > - SpotLight | Save a Spotlight HMI. |
IEC1131 TOOLSET - < Project:SpyList > - List of variables | Save the Spy List. |
Create program ' ProgN ' | Create a POU. |
Copy program ' ProgN ' to 'ProgNew ' | Copy the POU to the new POU name. |
Move or rename program ' ProgN ' (as 'NewName ') | Rename or modify the POU. |
Delete program ' ProgN ' | Delete the POU. |
ProgN : imported from project <Project> | Import the specified POU from another project. |
IEC1131 TOOLSET - <Project:Program> - Diary | Edit the Diary file for the specified POU. |
FBD/LD Program ' ProgN ' | Save the specified FBD or LD POU. |
SFC Program ' ProgN ' | Save the specified SFC POU. |
IEC1131 TOOLSET - < Project:Program > - ST Program | Save the specified ST POU. |
IEC1131 TOOLSET - < Project:Program > - Quick LD Program | Save the specified quick LD POU. |
IEC1131 TOOLSET - < Project:Program > - IL Program | Save the specified IL POU. IL POUs are not supported in AADvance-Trusted SIS Workstation software® . |
IEC1131 TOOLSET - < Project:Program > - Flow Chart | Save the specified FC POU. FC POUs are not supported in AADvance-Trusted SIS Workstation software . |
IEC1131 TOOLSET - < Project:Program > - Local messagesIEC1131 TOOLSET - < Project:Program > - Local timersIEC1131 TOOLSET - < Project:Program > - Local integers/realsIEC1131 TOOLSET - < Project:Program > - Local booleansIEC1131 TOOLSET - < Project > - Global messagesIEC1131 TOOLSET - < Project > - Global timersIEC1131 TOOLSET - < Project > - Global integers/realsIEC1131 TOOLSET - < Project > - Global booleans | Save variables having the specified local or global data type in the dictionary. |
IEC1131 TOOLSET - < Project:Program > - Local function blocksIEC1131 TOOLSET - < Project > - Global function blocks | Save local or global function block instances in the dictionary. |
IEC1131 TOOLSET - < Project:Program > - Local definesIEC1131 TOOLSET - < Project > - Global definesIEC1131 TOOLSET - < Project > - Common defines | Save local or global function block instances in the dictionary. |
Validator # Exit without viewing all dependency information Validator # Report printed to file Validator # Report sent to printer Validator # File scan complete Validator # File scan failed or aborted Validator # scanning TIC code: <project path> Validator # scanning file: <project path> | Validate various actions performed with these validators: Cross Reference Checker (#1) or TIC Dependency Checker (#2). |
TIP:
This list may not be exhaustive.
Provide Feedback