Cross Reference Checker
To access the Cross Reference Checker
From the
View
menu, point to Validators
, and then click Cross Reference Checker
.The
Cross Reference Checker
validates the cross reference file. This file is generated when updating the cross reference data displayed in the Cross Reference Browser
. The validator processes the file and graphically displays variable usage and program organization unit (POU) dependencies. Both shared and unshared variables and their associated POUs display in the tree hierarchy.The
Cross Reference Checker
displays:- POUs using variables
- The number of used variables
- The number of unused variables
- POUs with shared variables
- Shared variables
- Lines processed
POUs sharing one or more variables are dependent on each other. Modifications to one POU can affect the behavior of a dependent POU. For SIL3 safety applications, verify POU dependencies to ensure the target integrity of the application.
For a POU, the
Cross Reference Checker
identifies the POUs calling the POU and the POUs called by the POU, and shows the POUs that need verification. The validator also identifies the variable type and the quantity of POUs using a variable.The
Cross Reference Checker
is available from the AADvance-Trusted SIS Workstation software®
or as a stand-alone application. Update the cross reference data from the Cross Reference Browser
to use the Cross Reference Checker
.When viewing statistical information, display information for all POUs or only specified POUs or variables.
When viewing the graphical display of POU and variable dependencies, the icons in the tree hierarchy represent:
![]() | POU with no shared variables. Expand to display the non-shared
variables. |
![]() | POU with shared variables. Expand to display both shared and unshared variables. |
![]() | Unshared variable. Expand to display the associated POU name. |
![]() | Shared variable. Expand to display the names of all POUs sharing the variable. |
Perform these tasks with the
Cross Reference Checker
:Task | Procedure |
|---|---|
Validate the cross references data |
|
Expand or collapse the nodes in the POU dependency tree |
|
Print the validator results | Set the default printer to use the A4 paper format.
|
Provide Feedback




(or press
.
.