Validators
When creating
Trusted®
projects, use various validators to verify the application program code generated by the AADvance-Trusted SIS Workstation software®
. The validators process various database files produced by the AADvance-Trusted SIS Workstation software
to identify dependencies between programs within an application and the differences between versions of an application. For Trusted
applications, use the following four validators:- Cross Reference Checker
- TIC Dependency Checker
- TIC Difference Checker
- TIC Version Checker
When verifying the generated application code, the following files are used by the validators:
- APPLI.HIS, text file containing the history of the application
- appli.tst, file containing the symbolic information for variables and programs
- appli.X6M, file containing the generated target code. Set theEnable ISA68Mproperty toTrue.
- The following table displays the application files verified by each validator:ValidatorAPPLI.HISappli.tstappli.X6MCross Reference CheckerXTIC Dependency CheckerXXXTIC Difference CheckerXXTIC Version CheckerX
Provide Feedback