TIC Version Checker
To access the TIC Version Checker
From the View menu, point to
Validators
, and then click TIC Version Checker
.The
TIC Version Checker
compares the compiled TIC code generated by the AADvance-Trusted SIS Workstation software®
with the application downloaded onto the Trusted
processor. The TIC Version Checker
validates that the running application and the compiled TIC code are identical by displaying any differences between the TIC code of the applications.These conditions cause differences between the
Symbols CRC
, Application CRC
, and Total Size
of an application:- Modifications made by a user
- Unexpected changes caused by theAADvance-Trusted SIS Workstation software
- Recompiling the project, for the Application CRC only
To compare versions of an application, create a copy of the project running on the processor. The
TIC Version Checker
compares the copy of the project with the running application. The TIC Version Checker
displays differences caused by modifying the project application.The
TIC Version Checker
is available from the AADvance-Trusted SIS Workstation software
or as a stand-alone application. The
TIC Version Checker
displays these details:Program Name | The name of the project or application. |
|---|---|
Version | The version of the application extracted from the downloaded database file. |
Date | The last compilation date of the database file. |
Time | The last compilation time of the database file. |
Symbols CRC | Cyclic redundancy checking of the application symbols. Different applications may have matching Symbols CRC values if both applications contain the same symbols. |
Total Size | Size of the application in bytes. |
Application CRC | Cyclic redundancy checking of the downloaded TIC code. Recompiling a project changes the value of the Application CRC even when the application not modified. |
Perform these tasks with the
TIC Version Checker
:Task | Procedure |
|---|---|
Compare application TIC code with the TIC Version Checker | To compare versions of an application, create a copy of the project running on the processor. The TIC Version Checker compares the project copy with the running application. The TIC Version Checker displays differences caused by modifying the project application.
|
Print the validator results | Set the default printer to use the A4 paper format.
|
Provide Feedback