TIC Dependency Checker
To access the TIC Dependency Checker
From the
View
menu, point to Validators
, and then click TIC Dependency Checker
.The
TIC Dependency Checker
validates variable usage and program organization unit (POU) dependencies, and specifies POUs that need verification. Unlike the Cross Reference Checker
that also performs this validation, the TIC Dependency Checker
generates the dependency data from the downloadable TIC code and application symbols database files generated after compilation.The
TIC Dependency Checker
displays these statistics:- Total number of POUs
- POUs using variables
- Total number of variables
- POUs with shared variables
- Shared variables
- Total TIC codes
Perform an additional consistency check by comparing the displayed data using the
Cross Reference Checker
and the TIC Dependency Checker
.For a POU, the
TIC Dependency Checker
identifies the POUs calling the POU and the POUs called by the POU, and shows the POUs that need verification. The validator also identifies the variable type and the quantity of POUs using a variable. The
TIC Dependency Checker
is available from the AADvance-Trusted SIS Workstation software®
or as a stand-alone application. Successfully build the project to use the TIC Dependency Checker
.When viewing the statistical information, display information for all POUs or only specified POUs or variables.
When viewing the graphical display of POU and variable dependencies, the icons in the tree hierarchy represent:
![]() | POU having no shared variables. When expanded, displays the non-shared
variables. |
![]() | POU having shared variables. When expanded, displays both shared and unshared variables. |
![]() | Unshared variable. When expanded, displays the associated POU name. |
![]() | Shared variable. When expanded, displays the names of all POUs sharing the variable. |
Perform these tasks with the
TIC Dependency Checker
:Task | Procedure |
|---|---|
Validate the POU dependencies |
|
Expand or collapse the nodes in the POU dependency tree |
|
Print the validator results | Set the default printer to use the A4 paper format.
|
Provide Feedback




.
.