Enable power flow debugging
Use power flow debugging to follow the flow of logic during simulation or online debugging of LD/FBD programs. Power flow debugging provides a quick visual representation of signals.
By default, a red power flow line indicates True, while a blue power flow line indicates False.
Turn on power flow debugging for the
Trusted
device.
TIP:
While power flow debugging is enabled by default for
Trusted
Toolset projects, it is disabled by default in AADvance-Trusted SIS Workstation software
.To enable power flow debugging
- In theApplication View, right-click the device and then selectProperties.ThePropertieswindow opens.
- ExpandCompiler Options.
- SetGenerate Debug InfotoTRUE.
- In the menu, selectFile > Save Device.The power flow setting is saved.
Provide Feedback