Creating a Trusted Project
Trusted
ProjectCreate projects with the
AADvance-Trusted SIS Workstation software
. Also import projects created using the Trusted®
Toolset.Templates available for
Trusted
projects are:- Trusted, enables creating aTrustedproject containing one device in theAADvance-Trusted SIS Workstation software®.
- ImportTrustedToolset Project, enables importing aTrustedToolset project into theAADvance-Trusted SIS Workstation software.
Since the
Trusted
run-time is a 16-bit application, the quantity of program organization units (POUs), variables, and I/O modules are directly dependent upon that environment.For projects, the following properties are defined:
Property | Description |
|---|---|
File Encoding | The Windows character encoding to support text in editable project fields.
Autopopulated based on the Windows Language for non-Unicode programs
setting. Possible values:
Refer to Languages. |
Name | Name of the project. Project names are limited to 32 characters beginning with a letter or single underscore followed by letters, digits, and single underscores. The last character for a project name must be a letter or digit; project names cannot end with an underscore character. Names cannot be reserved words, defined words, or data types. |
Password Protected | Indication that the project is protected by a password controlling its access |
Path | Complete path where the project is stored on the computer. The path is automatically assigned: %USERPROFILE%\My Documents\SIS Workstation <version> \Projects\ProjectName |
Property | Description |
|---|---|
Documentation | Rich text |
Property | Description |
|---|---|
Permission Set | The FactoryTalk Directory Permission Set associated to the Trusted project. |
Perform the following tasks for projects:
- Accessing the properties of projects
- Building projects
- Cleaning projects
- Downloading project code
- Simulating projects
- Connecting projects
- Copying projects
Perform online updates for projects. Control access for projects by setting a password restricting modifications such as adding programs, functions, and function blocks.
To create a
Trusted
project- From theFilemenu, clickNew Project...(or pressCtrl+Shift+N).TheNew Projectdialog box is displayed.
- In theNew Projectdialog box, click thetab.Trusted
- In theProject Typeslist, click, and in theTrustedTemplateslist, click theCreate New Projecttemplate.
- Specify a name and comment for the project, and then clickOK.
Provide Feedback