Copy a Trusted project
Trusted
projectCreate a copy to rename a project.
To copy a
Trusted
project- In theApplication View, select the project.
- From theFilemenu, clickSave <Project>As....
- In theSave ProjectAs dialog box, do the following:
- Specify a name for the project.
- (optional) ClickBrowse...to specify the database path, and then clickOK.
- ClickSave.The selected project is copied and renamed.
Provide Feedback