To import a Trusted Toolset project
Trusted
Toolset projectImport projects created with the
Trusted®
Toolset. Choose to rename
the project when importing.To import a
Trusted
Toolset project- From theFilemenu, clickNew Project...(or pressCtrl+Shift+N).TheNew Projectdialog box displays.
- In theNew Projectdialog box, in the Project Types list, clickImport.
- In theTemplateslist, clickImport.TrustedToolset Project
- Specify a name for the project, and then clickBrowseto select the database path.
- In theSelect Projectdialog box, locate and select the project database file (appli.hie), and then clickOpen.
- A message may display asking to update the database to the current version. After updating the database, a previous version of theTrustedToolset can no longer open the project. To continue the importation process, clickOK.
- In theNew Projectdialog box, clickOK.TIP:AADvance-Trusted SIS Workstation softwareopens one project at a time. After making changes to a project, the system automatically prompts to save changes before closing the project or opening another.
Provide Feedback