Restore a Trusted project
Trusted
projectRestore a
Trusted
project to open a snapshot of its Windows’ folder at
the time of archival. The restored project contains all code, comments, modification
history, documentation, and compiled binaries created by the project at the time of
archival.
IMPORTANT:
Archived projects are not encrypted and should not be used to store or
transmit sensitive information over unencrypted protocols.
The Global Library is not
included in archived projects. Take appropriate steps to ensure that the restored project
is compatible with the Global Library that is used to restore the project. For example,
the archived project should be shared along with the Global Library program organization
unit (POU).
To restore a project:
- SelectFile > New Project.
- InNew Project, from theTrustedtab, selectProject Types > Restore.
- InTemplates, selectRestore Project from an Archive, then selectBrowse.
- InSelect Archive File, navigate to the project archive, then selectOpen.
- InNew Project, selectOK.
NOTE:
When restoring a project that was archived from a folder with a
depth level different than the depth level of the Projects location folder, it must be
rebuilt to connect to the physical controllers or to go into simulation.
When a project is
restored from the Projects location folder,
AADvance-Trusted SIS Workstation software®
downloads, updates, and connects to the controller without having to build the
project. Provide Feedback