Dictionary
Use the
Dictionary
to manage variables and defined words. Create, edit, or delete variables and defined words from the dictionary instances. The grids of the Dictionary include: - Defined Words grid -- manages the defined words for a project. For example, create the defined wordOKto replace the boolean value TRUE in program organization units (POUs).
- Variables grid -- manages the variables for POUs and the device. Each device and POU has its instance of the grid. For the device, the grid displays global variables. For POUs, the grid displays local variables.
Open the dictionary grids from the
Application View
. The grids each display the properties for the local variables, global variables, or defined words. Open multiple grids simultaneously.Customize the
Dictionary
environment by arranging the columns to display and setting the display colors.To arrange the columns to display
IMPORTANT:
To retain customized display settings, save the
Dictionary
instance before closing.- To move a column, drag the column header to another location.When dragging a column header, arrows indicate the current position of the header.
- To hide a column, right-click a column header, and then clickHide Column.
- To show a column, right-click any column header, point toShow Column, and then click the required column name.
Provide Feedback