Access a Dictionary grid instance
Manage global variables, local variables, or defined words from the Dictionary instances to configure the program organization units (POUs) in a project.
To access a Dictionary grid instance
- From theApplication View, expand the device node and double-clickGlobal Variables. The Dictionary instance appears and contains the global variables belonging to the device.
- For the variables of a POU, expand the required POU node and double-clickLocal Variables. The Dictionary instance appears and contains the variables belonging to the POU.
- For the defined words of a project, double-clickDefined Words. TheDefined Wordsgrid appears.
Provide Feedback