Variable extended attributes
Extended attributes allow the collection of appropriate data from the controller via the TMR Communications Interface module.
- In theSOEtab, generate a time-stamped log of all faults, field trips, output actions etc. recorded by the 8000 Series System. For details, see theTrustedSOE & Process Historian Software Package, publication ICSTT-RM243.TIP:
- You do not need to download code to the controller or update the running application if you change only the Message True and Message False variable properties in the global dictionary. When you connect with the controller, a confirmation message that indicates a mismatch appears. SelectYesto continue connecting with the controller.
- Download code to the controller or update the running application when you change only the Message True and Message False variable properties by using the variables data file.
- In thetab, control the manner in which data is controlled and interpreted overModbus®Modbuscommunications.
Provide Feedback