Select Boolean and Analog variables for SOE collection

Collect a time-stamped log of all faults, field trips, output actions and more recorded by the 8000 Series System:
  • Inherent Sequence of Events (SOE) logging of all Boolean type input states
  • Time resolution to 1ms
  • User-defined tag, description, state and display colors
  • Text-based log file for import into other programs
    TIP: For details, see the
    Trusted
    SOE & Process Historian Software Package Product Description, publication ICSTT-RM243.
To select Boolean and Analog variables for SOE collection
  1. Create a variable in the
    Dictionary
    .
  2. Wire the variable through the
    I/O Wiring
    tool.
  3. In
    Application View
    , right-click the dictionary instance, then select
    Extended Attributes
    .
  4. In
    Extended Attributes
    , in the
    SOE
    tab, click
    Add Variable
    .
  5. In the
    Variable Selector
    , select the variable to include in the SOE log.
  6. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal