Set an Intermediate variable for SOE collection without extended variables
An alternate method is available to collect data from the controller without using SOE extended attributes.
TIP:
For details, see the
Trusted
SOE
& Process Historian Software Package, publication ICSTT-RM243.
IMPORTANT:
Do not select a variable already using the SOE
extended attributes.
To set an Intermediate variable for SOE collection without extended variables
- Open theI/O Wiringtool.
- Add a SOE board.
- Double-click an unwired channel.
- In theVariable Selector, select the variable for the channel.
- ClickOK.The channel’sNamefield indicates the wired variable.
Provide Feedback