Set extended attributes for
Modbus
collection

Control the manner in which data is controlled and interpreted over
Modbus®
communications.
TIP: Extended attributes are only available for variables with a
Modbus
address. Specify the
Modbus
address format (
Hexadecimal
or
Decimal
) in the CAM
Trusted
settings from the
Tools
>
Options
menu. The
System Configuration Tool
reads
Modbus
addresses for variables in Decimal format.
  • Write Protect
    : Inhibits external communications from overwriting a data point. This applies to both Integer/Real and Boolean variables.
    To force compatibility of read/write capabilities of coils and registers for the current
    8110
    Trusted
    TMR Processor
    with previous firmware versions, when configuring the processor, in the
    Updater
    section, select the
    Auto Protect Network Variables
    check box. The compatible read/write capabilities of the coils and registers are the following:
    Address
    Element
    Number of Elements
    Capability
    00001 – 7500
    Coils
    (7500 coils)
    Read only
    07501 - 10000
    Coils
    (2500 coils)
    Read/write
    40001 - 47500
    Holding registers
    (2500 holding registers)
    Read only
    47501 - 50000
    Holding registers
    (2500 holding registers)
    Read/write
  • Registers as Unsigned Integer
    : Reads and writes
    Modbus
    data as unsigned data. Integer data is normally treated as 32-bit signed within the application (for signed data, the most significant bit is used to distinguish positive and negative numbers).
  • Use Two Registers (32-bits)
    : Uses two contiguous
    Modbus
    registers to transfer all 32 bits. By default, only the lower 16 bits of an analog data point are transferred to and from the
    Modbus
    communications.
  • Least Significant Word First
    : Reverses the words on the
    Modbus
    addresses. If
    Use Two Registers
    is selected, by default the most significant 16-bit word is addressed first on
    Modbus
    communications.
For details on extended attributes for
Modbus
variables, refer to the Product Description PD-8082,
Trusted
Toolset Suite.
To set extended attributes for
Modbus
collection
  1. In the
    Dictionary
    , select the variable, then set
    Modbus
    Address
    .
    TIP: The
    T8151 Communications Interface
    does not support duplicate
    Modbus
    addresses.
  2. Click
    OK
    .
  3. In the
    Application View
    , right-click the dictionary instance and click
    Extended Attributes
    .
  4. In the Appli.vxa window, select the
    Modbus
    tab, then select one or more of the extended attributes for the variable.
    TIP: The
    Least Significant Word First
    option is grayed out unless the
    Use Two Registers
    option is selected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal