Change the properties of a variable
Change the properties of an existing variable to accommodate the requirements of program organization units (POUs), I/O wiring, and
Modbus®
communication. For example, change the Direction
property for I/O wiring.
TIP:
Update each instance of a function or function block
after adding, removing, renaming, changing data type, or changing direction of parameters in
all POUs using the instance. Identify these POUs with the
Cross Reference Browser
,
then open each POU and reselect the modified instance using the Block
Selector
.To change the properties of a variable
- From theApplication View, double-click the Dictionary instance for the device or POU.
- In theVariables Grid, change the properties for the variable:
- Name
- Data Type
- String Size
- Attribute
- Direction
- Modbus Address
- Message True
- Message False
- Retained
- Initial Value
- Unit
- Comment
Provide Feedback