Running an Application Online
Running online means an application is connected to the physical
Trusted®
controller. AADvance-Trusted SIS Workstation software®
ensures the execution of the application code. While running online, force the values of variables and monitor the values of variables.Before running an application on a
Trusted
controller, build the project code and download the application code onto the target.For debugging purposes, simulate the running of an application. The compiler generates different code for simulation than when online.
Status information for the
Trusted
controller appears in the Application View
as a lightning bolt icon:![]() | When the icon is yellow, the Trusted controller is connected or
in simulation mode. |
From the
Application View
, view detailed status information for the Trusted
controller, including the identity of the AADvance-Trusted SIS Workstation software
locking the controller, by hovering over the controller status icons.When connected, the
Application View
displays states for the device:![]() | The device is running on the target. The device is in the RUN, STOP, or ERROR state. |
![]() | The device is not running on the target or no code is available on the target. The device is in the DISCONNECTED or NO APPLICATION state. |
The state of the device appears next to the device icon in the
Application View
:Device State | Description |
|---|---|
RUN | The device is running in real-time mode. The state of a device when online. |
DISCONNECTED | Unable to establish communication with the target device. Verify communication settings such as IP address. |
NO APPLICATION | The device is not running on the target. Possible reasons:
|
Provide Feedback