Download code to Trusted controllers
Trusted
controllersPerforming a download operation verifies that the latest build reflects the current project. Perform download operations for projects with code to send to physical
Trusted
controllers. When simulating, do not perform download operations. Prerequisites
- Connect the computer where theAADvance-Trusted SIS Workstation softwareis installed to the hardware controller through a Serial or Ethernet network.
To download project code
- In thePropertieswindow for the device, configure these properties:
- Enable ISA68M
- Host Address
- Host Socket PortTIP: The compiler generates different code for simulation than for targets.
- Build the project code.
- Set the maintenance enable key switch on theTrustedcontroller to theMaintainposition.
- From theApplication View, right-click the project element, and then selectDownload.
Provide Feedback