Start or stop a Trusted controller
Trusted
controllerStop or start the application running the
Trusted
controller from the AADvance-Trusted SIS Workstation software®
.- Stopping the execution of the application causes theTrustedcontroller to go into the configured safe state.
- Starting the execution of the application causes the output to energize depending on the programmed logic conditions.
- Starting or stopping the application is only available when online.
Start or stop a
Trusted
controller- Connect to the application.
- From theOnlinemenu, clickStart applicationorStop application.
The application running on the
Trusted
controller stops or starts.Provide Feedback