Setting Project Access Control
For project security, set access control using a password for projects. Password definitions are limited to eight characters and can consist of letters, digits, and symbols. Enter the password to open a password-protected project.
In the
Application View
, the following indicates the security state:
A lock is applied to the
project.Edit existing passwords for projects or remove existing passwords. When copying, pasting, and importing projects having access control, password definitions are retained.
Task | Procedure |
|---|---|
Set a password |
|
Edit a password |
|
Remove a password |
|
Provide Feedback